Skip to main content
BWeng.1
Visitor II
February 7, 2021
Question

When using the STUSB4710 we want to be able to update the POD power level in real time. For example, if we change the POD5 current capability during normal option, will the downstream device know that the contract has changed adjust their sink settin

  • February 7, 2021
  • 0 replies
  • 786 views

Do we need to do a software reset or any additional function in order to trigger the downstream device to adjust their sink settings and reset the power contract that is in place? Or is the power contract automatically renegotiated when the POD current setting is updated via I2C?

    This topic has been closed for replies.