X-NUCLEO-67W61M1 uart connection for AT commands
How do I connect to the X-NUCLEO-67W61M1 uart in order to access the 'AT' commands?
I never get the AT> command prompt, although I get the bootup output spew, see below sample. I have tried 2 different uart-to-usb interface boards that work on other systems, so I have confidence in them.
The commands are documented here: http://wiki.st.com/stm32mcu/wiki/Connectivity:ST67W611M_AT_Command
My setup uses the X-NUCLEO-67W61M1 expansion board with the Nucleo-H7S3L8 host board, and I successfully built and run the ST67W6X_CLI sample application. Both boards have the default configuration for the solder bridges. I know I can use the CLI sample app for 'AT' commands, but that is through the host board, and not what I am asking.
I have also been able to connect a serial interface interface to the TX & RX connectors at either the CN7 or CN9, on the X-NUCLEO-67W61M1 and get the bootup output on my terminal emulator. Contrary to the documents I could find, I had to use baud rate 2000000 (instead of 921600, which outputs bad characters). On Ubuntu I use the command sudo putty /dev/ttyUSB1 -serial -sercfg 2000000,8,n,1,N
Here is the beginning of the many lines of bootup output I see. But it does not respond to any input that I try to type in after bootup, nor does it give me a prompt for the AT> commands.
custom 0x0
flash init 0
Boot2 start:Apr 11 2025,11:39:40
Group=1,CPU Count=1
ver:8.1.9
user_fw
lp_fw not found
Active PT:0,Age 0
read mfg flag addr:1c6000
entry ID 0 found
Boot start
Media boot main