Accelerometer zero-g level change over time
Hi,
I am using IIS2ICLX MEMS accelerometer in an IOT device.
The IIS2ICLX is soldered on a PCB that sends data to internet every 10min.
To measure the zero-g level of both x and y axis, I suspend the device from the ceiling so that the PCB (and the accelerometer) is perfectly horizontal and and vibration-free.
I noticed that the zero-g level changes if I briefly touch the device, and wait for the device to return to its horizontal position (the temperature of the device does not change).
Does anyone has an explanation ?
I there a way to minimize this effect by using two redondant accelerometers, with a 90 degre rotation between them ?
Thanks for your help.