Skip to main content
dmeise
Associate
July 27, 2023
Solved

AIS2DW12 Zero-g level offset accuracy, long term

  • July 27, 2023
  • 2 replies
  • 1209 views

Can anyone tell me how to understand the following parameter out of the AIS2DW12 datasheet.
Zero-g level offset accuracy, long term: ± 700mg

When i use the sensor with a resolution of ± 2g, then I hope there ist not the possibility that the offset will drift this far. 

 

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @dmeise ,

If +/-700mg is too much for you, have a look at our AIS2IH which has zero-g level offset accuracy, long term of +/- 300mg, it is  designed to address non-safety automotive applications as AIS2DW12.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.

2 replies

TDK
Super User
July 27, 2023

Yep, ±0.7g offset when the full scale is ±2g is a lot, but that's what it is.

TDK_0-1690462182180.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Federica Bossi
Federica BossiBest answer
Technical Moderator
July 28, 2023

Hi @dmeise ,

If +/-700mg is too much for you, have a look at our AIS2IH which has zero-g level offset accuracy, long term of +/- 300mg, it is  designed to address non-safety automotive applications as AIS2DW12.

If this helps you, please mark my answer as "Best Answer" by clicking on the "Accept as Solution" button, this can be helpful for Community users to find this solution faster.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.