Skip to main content
Thomas L.
Associate III
February 1, 2023
Solved

Any examples available for SFLP (Sensor Fusion) in LSM6DSV16X sensors

  • February 1, 2023
  • 3 replies
  • 3382 views

Hi

I was wondering if there are any examples for using the Sensor Fusion Low Power Algorithm inside a LSM6DSV16X. I would like to retrieve the current Heading, Pitch and Roll information. Alternatively I'd also be happy with an example explaining how to get the Quaternion values from the SFLP. Anything regarding the SFLP would be nice. The examples do not outline any of the SFLP features (at least I was unable to find anything except the calls for directly manipulating the registers).

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @TLi.7nder​ ,

    You can have a look to the C examples for the use and configuration of SFLP in LSM6DSV16X sensors on Github at this link --> lsm6dsv16x_sensor_fusion.c

    -Eleon

    3 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    February 2, 2023

    Hi @TLi.7nder​ ,

    You can have a look to the C examples for the use and configuration of SFLP in LSM6DSV16X sensors on Github at this link --> lsm6dsv16x_sensor_fusion.c

    -Eleon

    FKara.3
    Associate III
    August 8, 2023

    https://github.com/stm32duino/LSM6DSV16X/blob/main/src/lsm6dsv16x_reg.c

    Is there a sensor fusion configuration available on GitHub for Arduino? If not, are there any plans to add it in the future?

    KWine
    Senior
    October 1, 2023

    Here is an Arduino example.

    Thomas L.
    Thomas L.Author
    Associate III
    February 2, 2023

    @Eleon BORLINI​ 

    Eleon, I am so sorry. I had cloned the repository and even checked out the examples for the lsm6dsv16x but apparently I was blind.

    FKara.3
    Associate III
    October 2, 2023

    Thanks @KWine ,

    Also, An Arduino Sensor fusion example for lsm6dsv16x has recently been added to GitHub.  If you interested, here is the link