Skip to main content
lucky chong
Visitor II
January 10, 2023
Solved

Are the three axes of LIS3MDL orthogonal?

  • January 10, 2023
  • 1 reply
  • 906 views

As far as I know, the LIS3MDL is an excellent 3-axis tmr sensor.

What I want to know is whether the magnetic field components of the XYZ axes measured by the LIS3MDL sensor are strictly orthogonal, and do I need to do some calibration before using it?

Thanks�?

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @lucky chong​ ,

    the LIS3MDL aces are orthogonal, but the device could be for example mounted tilted, or there could be external stresses affecting the internal axis orthogonality.

    For this reason, we always suggest a calibration at application level.

    See for example the MotionMC magnetometer calibration library in X-CUBE-MEMS1 expansion for STM32Cube.

    -Eleon

    1 reply

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    January 20, 2023

    Hi @lucky chong​ ,

    the LIS3MDL aces are orthogonal, but the device could be for example mounted tilted, or there could be external stresses affecting the internal axis orthogonality.

    For this reason, we always suggest a calibration at application level.

    See for example the MotionMC magnetometer calibration library in X-CUBE-MEMS1 expansion for STM32Cube.

    -Eleon