Skip to main content
Visitor II
November 3, 2024
Question

ASM330LHB performance?

  • November 3, 2024
  • 1 reply
  • 560 views

Hello,

ASM330LHB 6-axis sensor, can it reach 0.001g?

ASM330LHB 6-axis sensor that can reach 0.001g? how high can it reach?

Which 6-axis sensor is more accurate?

Can they both output angles?

 

This post has been translated from Chinese to comply with the ST Community guidelines.

 
 

1 reply

Federica Bossi
Technical Moderator
November 8, 2024

Hi @1232 ,

The maximum value that the sensor can reach and also the accuracy depend on the full scale you set according to datasheet:

FedericaBossi_0-1731073939188.png

If you want to reach higher g you can look at LSM6DSV32X that has a maximum full scale of 32g, but not that it is not for ASIL B automotive applications.

Can they both output angles? Yes.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.