Skip to main content
Associate
January 16, 2025
Question

Automated data acquisition at regular time intervals on STWINKT1B

  • January 16, 2025
  • 1 reply
  • 508 views

Hello, I am currently working on a project concerning the degradation of a rotary machine overtime. To detect this degradation, we want to study vibration using the IIS3DWB accelerometer which is on the STWINKT1B. Till now, I am taking 30 seconds of data "manually" every 2 days by using the ST BLE Sensor app. With those data I am checking the evolution of the spectrum to try to find a pattern.

I was wondering if it is possible to make the acquisition process automatic and if yes how.

For now, I am using the firmware FP-SNS-DATALOG2_Datalog2. I have very little knowledge in firmware programming so if you can use a simple language in your answer I would really appreciate it :) 

1 reply

Andrew Neil
Super User
January 16, 2025

 


@fast_red_LED_enjoyer wrote:

I was wondering if it is possible to make the acquisition process automatic and if yes how. 


Sure. You need to create firmware which does that - it's all open-source.

 


@fast_red_LED_enjoyer wrote:

I have very little knowledge in firmware programming  :) 


Well, this is a firmware programming task!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.