Skip to main content
Associate III
May 23, 2024
Solved

Can i use multiple sensors of the same type simultaneously to improve measurement quality?

  • May 23, 2024
  • 1 reply
  • 1120 views

My question is, using Algobuilder (or mems studio) and unicleo, can i use for example two accelerometers (on hardware nucleo 401RE, x-nucleo ISK01A3 and steval MKI233) and get data from them simultaneously to reduce the measurement error/noise?

Whats the best option for this to be made?

Thanks in advance

Best answer by Federica Bossi

Hi @aesteban ,

Welcome to ST Community!

Unfortunately, this is not possible in AlgoBuilder or any other FW.

A solution you could try is to generate Datalogterminal firmware using CubeMX and X-CUBE-MEMS1 package. But it will send the data to terminal.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
May 28, 2024

Hi @aesteban ,

Welcome to ST Community!

Unfortunately, this is not possible in AlgoBuilder or any other FW.

A solution you could try is to generate Datalogterminal firmware using CubeMX and X-CUBE-MEMS1 package. But it will send the data to terminal.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.