Skip to main content
Associate II
September 10, 2024
Solved

Can the LPS27HHW be used to detect non-water liquids, such as oil?

  • September 10, 2024
  • 1 reply
  • 628 views

Hi Sir,

 

Can the LPS27HHW be used to detect non-water liquids, such as oil?

 

 

Best answer by Federica Bossi

Hi @TIENHUA ,

Theoretically it is possible to see other liquid respect to water. The only issue is due to chemical material is present into the liquid you are referring. This can cause a damage of the gel present in the device. In case of some particles passes the gel, the device doesn't work properly. The suggestion is to test the device in desired liquid.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
September 19, 2024

Hi @TIENHUA ,

Theoretically it is possible to see other liquid respect to water. The only issue is due to chemical material is present into the liquid you are referring. This can cause a damage of the gel present in the device. In case of some particles passes the gel, the device doesn't work properly. The suggestion is to test the device in desired liquid.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.