Skip to main content
Associate
October 6, 2023
Question

Cannot conect to STEVAL-STWINBX1

  • October 6, 2023
  • 1 reply
  • 983 views

Hello, 

I have received the STEVAL-STWINBX1 evaluation kit and am trying different demos to see how it works. 

At first I was programming the board with different examples (STM32CubeFunctionPack_STBOX1_V1.5.0) but I was having problems afterwards. Once the programming was done, I was trying to connect to the board via BLE Sensor App but my board didn't appear until I pressed RESET. Then, I read an issue on this community where a user was having a similar problem and the solution was to program the binary file on Bank 2 (Start address: 0x08100000). 

The problem still persists but now, once I connect the board to my computer, the computer doesn't detect it and the only LED blinking is LED_C. I don't know what to do, because I can't reset the board and I can't connect it to the computer either to program it again... 

Any suggestions?

This topic has been closed for replies.

1 reply

aagAuthor
Associate
October 6, 2023

Forgot to say I'm trying to detect the board with the computer pressing USER button before connecting it to the computer, but still it doesn't work.