Skip to main content
Abishek Devan
Associate
February 13, 2023
Solved

Conformal coating - LIS2DW12TR

  • February 13, 2023
  • 2 replies
  • 1147 views

Hi Team

We are currently working on ST PN: LIS2DW12TR in our new project. Thus, I would like to check with ST whether this part is OK to be Conformal coated? The reason is, our PCB will need to be conformal coating after all the components are populated on it. Hence would like to understand if there is any risk for this ST component to go thru this conformal coating process.

Regards,

Abishek

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Abishek Devan​ ,

    There is in principle no issue, if the temperature of conformal coating deposition doesn't exceed the maximum absolute ratings of 125°C for long time. My suggestion is however to calibrate the part in the software after soldering + conformal coating before starting using it.

    -Eleon

    2 replies

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    February 13, 2023

    Hi @Abishek Devan​ ,

    There is in principle no issue, if the temperature of conformal coating deposition doesn't exceed the maximum absolute ratings of 125°C for long time. My suggestion is however to calibrate the part in the software after soldering + conformal coating before starting using it.

    -Eleon

    Abishek Devan
    Associate
    February 13, 2023

    Thanks for the clarification Eleon.