Skip to main content
Visitor II
February 2, 2024
Question

Does the Mems sensor LPS22HBTR require exercising before first use?

  • February 2, 2024
  • 1 reply
  • 830 views

Does the Mems sensor LPS22HBTR require exercising before first use? Our company uses these for detectioopn of objects hitting a membrane and we have come to find out that it appears the mems sensor sometimes needs a puff of air in order to begin working correctly. Is this true, is there some kind of standard first time procedure before using the sensor that I am not aware of?

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
March 6, 2024

Hi @jeffgedgaud ,

Welcome to ST Community!

LPS22HB is able to works without any specific "exercise". What has been highlighted seems due the fact that some undesired particles close the holes present over the device. These holes must be left free to avoid to creates wrong measurements. If the problem exists at first power on, this means that the problem could be in soldering (or cleaning) phase where sometimes wet cleaning is used. In LPS22HB, wet soldering (also with flux) and wet cleaning is forbidden to avoid damage of holes. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.