Skip to main content
Associate II
October 17, 2023
Question

H3LIS331DL

  • October 17, 2023
  • 1 reply
  • 1008 views

Hi,

I'm Working with H3LIS331DL Accelerometer and STM32F410 for vibration test(Levels:0.04 g^2/Hz,2O Hz to 2000 Hz All 3 Axis, 5 Minutes each axis) at SPI mode.I have readed the raw data from the H3LIS331DL and communicated it by  UART. But after that,I have no idea how to use my raw data for my project requirement,can someone help me with this.About,How the raw Data conversion has been done and about the different output units of Accelerometer(for example-g,mg/digit.m/s^2). Thanks in advance.

This topic has been closed for replies.

1 reply

TDK
Super User
October 17, 2023

1 g = 9.8 m/s^2

1 mg = 0.001 g

"If you feel a post has answered your question, please click ""Accept as Solution""."