Skip to main content
HWäck.1
Associate
April 19, 2022
Solved

Hi there I am using a lsm6dsr to measure acceleration and gyrodata. I programed the write, read, delay and print functions ans validated them. But unfortunatly i can no get any values or activityfunctions from it.

  • April 19, 2022
  • 3 replies
  • 1658 views

I initialize the sensor like this:

uint8_t rst;
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &SENSOR_BUS;
static uint8_t whoamI;
/* Wait sensor boot time */
platform_delay(1000);
/* Check device ID */
lsm6dsr_device_id_get(&dev_ctx, &whoamI);
 
if (whoamI != LSM6DSR_ID)
	while (1);
 
/* Restore default configuration */
lsm6dsr_reset_set(&dev_ctx, PROPERTY_ENABLE);
 
do {
	lsm6dsr_reset_get(&dev_ctx, &rst);
} while (rst);
 
/* Disable I3C interface */
lsm6dsr_i3c_disable_set(&dev_ctx, LSM6DSR_I3C_DISABLE);
/* Enable Block Data Update */
lsm6dsr_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/* Set Output Data Rate */
lsm6dsr_xl_data_rate_set(&dev_ctx, LSM6DSR_XL_ODR_12Hz5);
lsm6dsr_gy_data_rate_set(&dev_ctx, LSM6DSR_GY_ODR_12Hz5);
/* Set full scale */
lsm6dsr_xl_full_scale_set(&dev_ctx, LSM6DSR_2g);
lsm6dsr_gy_full_scale_set(&dev_ctx, LSM6DSR_2000dps);
 /* Configure filtering chain(No aux interface)
* Accelerometer - LPF1 + LPF2 path
*/
lsm6dsr_xl_hp_path_on_out_set(&dev_ctx, LSM6DSR_LP_ODR_DIV_100);
lsm6dsr_xl_filter_lp2_set(&dev_ctx, PROPERTY_ENABLE);

Then i periodicly try to read the sensors data:

uint8_t reg;
 /* Read output only if new xl value is available */
lsm6dsr_xl_flag_data_ready_get(&dev_ctx, &reg);
 
if (reg) {
/* Read acceleration field data */
 memset(data_raw_acceleration, 0x00, 3 * sizeof(int16_t));
 lsm6dsr_acceleration_raw_get(&dev_ctx, data_raw_acceleration);
 acceleration_mg[0] =
 lsm6dsr_from_fs2g_to_mg(data_raw_acceleration[0]);
 acceleration_mg[1] =
 lsm6dsr_from_fs2g_to_mg(data_raw_acceleration[1]);
 acceleration_mg[2] =
 lsm6dsr_from_fs2g_to_mg(data_raw_acceleration[2]);
 sprintf(tx_buffer,
 "(IMU) Acceleration [mg]: %4.2f\t%4.2f\t%4.2f\r\n",
 acceleration_mg[0], acceleration_mg[1], acceleration_mg[2]);
			PRINTF("%s", tx_buffer);
 }
 
lsm6dsr_gy_flag_data_ready_get(&dev_ctx, &reg);
 
if (reg) {
 /* Read angular rate field data */
 memset(data_raw_angular_rate, 0x00, 3 * sizeof(int16_t));
 lsm6dsr_angular_rate_raw_get(&dev_ctx, data_raw_angular_rate);
 angular_rate_mdps[0] =
 lsm6dsr_from_fs2000dps_to_mdps(data_raw_angular_rate[0]);
 angular_rate_mdps[1] =
 lsm6dsr_from_fs2000dps_to_mdps(data_raw_angular_rate[1]);
 angular_rate_mdps[2] =
 lsm6dsr_from_fs2000dps_to_mdps(data_raw_angular_rate[2]);
 sprintf(tx_buffer,
 "(IMU) Angular rate [mdps]: %4.2f\t%4.2f\t%4.2f\r\n",
 angular_rate_mdps[0], angular_rate_mdps[1], angular_rate_mdps[2]);
			PRINTF("%s", tx_buffer);
 }
 
 lsm6dsr_temp_flag_data_ready_get(&dev_ctx, &reg);
 
 if (reg) {
 /* Read temperature data */
 memset(&data_raw_temperature, 0x00, sizeof(int16_t));
 lsm6dsr_temperature_raw_get(&dev_ctx, &data_raw_temperature);
 temperature_degC = lsm6dsr_from_lsb_to_celsius(
 data_raw_temperature);
 sprintf(tx_buffer, "(IMU) Temperature [degC]: %6.2f\r\n",
 temperature_degC );
			PRINTF("%s", tx_buffer);
 }

"reg" is always zero, thats why it never enters the if-statement to get the data. But even when i force the code to enter the if-statement it just returns 0.00 0.00 0.00.

I also tried to get activitydata with the same behaviour.

Does anyone of you see what's missing in my code?

    This topic has been closed for replies.
    Best answer by HWäck.1

    Hi Eleon

    I found out that only the readfunction was working properly. Now the writefunction is also working and lets me read data from the sensor

    3 replies

    Eleon BORLINI
    ST Employee
    April 22, 2022

    Hi @Hannes Wäckerlig​ ,

    which hardware platform are you using in you application?

    Are you using I2C or SPI? And did you check the goodness of the signal with an oscilloscope?

    -Eleon

    HWäck.1
    HWäck.1AuthorBest answer
    Associate
    April 25, 2022

    Hi Eleon

    I found out that only the readfunction was working properly. Now the writefunction is also working and lets me read data from the sensor

    Eleon BORLINI
    ST Employee
    April 26, 2022

    Hi @Hannes Wäckerlig​ 

    glad you found and shared the solution to the issue!

    Best,

    -Eleon

    DSaci.2
    Associate II
    December 4, 2022

    Hi @Hannes Wäckerlig​ ,

    I am having the same issue. The write won't work. What did you do to get it to work

    thanks,

    Don