Skip to main content
Associate
January 9, 2024
Question

High Frequency Noise From STWINMA2A

  • January 9, 2024
  • 2 replies
  • 1244 views

Hello everyone,

I am currently working with STWIN+STWINMA2A microphone array for ultrasonic signal processing. I use the firmware "AMicArray_Microphones_Streaming" and connect the board directly to my laptop as an USB microphone.

However, the data suffers from significant noise with certain frequencies.

I used Audacity to sample the data in an quiet environment, with the configuration as figure 1. The sampling rate is 96kHz.

xiaohangz_0-1704828877639.png

The DFT of 10,000 data points is shown in the next figure, we can see a very high noise level at around 40k, 24k, and 8kHz.

xiaohangz_1-1704828956551.png

Is there any thing I can do to fix this problem?

Thanks!

 

 

This topic has been closed for replies.

2 replies

AScha.3
Super User
January 9, 2024

Hi,

STWINMA2 is analog mic array - why an array , not just one mic ?

+

Is analog out - whats the preamp ? and the ADC ? any spec about noise and SFDR ?

+

Did you look at the signal at the adc input with a scope ? 

"If you feel a post has answered your question, please click ""Accept as Solution""."
xiaohangzAuthor
Associate
January 10, 2024

Hi

 

With an array, I will be able to estimate the direction of signal arrival. Also, STWINMA2 is able to perform beamforming for ultrasonic signals less than 40kHz.

 

About preamp and other specs, I have not divided into them. You are right I need to check those carefully also look at the signal with a scope.

 

I will attempt to replace the cable and move away form my lab tomorrow. There might be high frequency electromagnetic ghosts in my lab.

 

Thanks.

Federica Bossi
Technical Moderator
February 1, 2024

Hi @xiaohangz ,

Did you solve?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.