Skip to main content
BSeeg
Associate
January 23, 2023
Question

how can i change the STEVAL-MKI109V3 VDDIO to 3.3 V or get the INT1_up or INT2_up signals with an 3.3V Level?

  • January 23, 2023
  • 2 replies
  • 656 views

..

    This topic has been closed for replies.

    2 replies

    Peter BENSCH
    Technical Moderator
    January 23, 2023

    Welcome, @BSeeg​, to the community!

    you can use the command *setvddio3.3 to set VDDIO=3.3V. This and all other commands are listed in UM2116.

    Hope that helps?

    Regards

    /Peter

    BSeeg
    BSeegAuthor
    Associate
    January 23, 2023

    Hello Peter

    Is there a way to send comands in the unico Gui?

    I tested The UART Interface and only the command

    "*list"

    did somthing

    the Command

    "*setdbMKI195V1" to select the LSM6DSRX Sensor i use got an

    "inf Adapter nor supported" response

    The conds *setvddio3.3 or *setvdda3.3 changed nothing nor got an response.

    best regards Bene