Skip to main content
shenghua yang
Associate III
March 1, 2023
Question

How to add FFT algorithms in the AMICAM1\Microphones_Streaming based on NUCLEO-STM32L476RG ?

  • March 1, 2023
  • 4 replies
  • 1536 views

..

This topic has been closed for replies.

4 replies

shenghua yang
Associate III
March 1, 2023

Dear All:

I would like to add FFT algorithms in the "AMICAM1\Microphones_Streaming" based on NUCLEO-STM32L476RG ?

From the document of UM1901, we can get audio data in the callback function(AMICAM1_AUDIO_IN_TransferComplete_CallBack) per 1 msec with 192KHz of samping rate as below.

0693W00000aHvU1QAK.pngWe hope to save 6 msec of audio data in the PCM_Buffer(192*6=1152, 24 bits of data) from AD1974 for FFT analysis.

When finishing the 1152 bytes of audio data collection, we normalize transfer 24 bits audio data into the range of +/- 1 audio signal for implementing FFT analysis.

We also can find the fft.c in the library of middle ware as below.

0693W00000aHvfYQAS.png

There are some FFT API in a compiled HTML file located in the Documentation folder.

0693W00000aHvjQQAS.png

How to implement the 1024 point of FFT algorithms step by step?

Best Regards,

Sheng-Hua

SimonePradolini
Technical Moderator
March 2, 2023

Hello @shenghua yang​ 

X-CUBE-MEMSMIC1 already provides an example using FFT.

Is it called UltrasoundFFT and it is placed here: Projects\STM32L476RG-Nucleo\Demonstration\AMICAM1\UltrasoundFFT\.

Start looking at this code example, that is fully working and already provides what you need.

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
shenghua yang
Associate III
March 3, 2023

Dear Simone:

Thanks your help.

We have found the ​UltrasoundFFT and successfully compiles the project.​

It runs a 512 points of FFT algorithm with 50% of overlapping.

 FFT_Lib_Init(512, 0.5f);

Which microphone(M1,M2,M3,M4) elements are used to do FFT in this project?

void AMICAM1_Data_Ready(uint8_t *buf, uint16_t size, double timeStamp)

{

 FFT_Lib_Data_Input((int16_t *)buf, size / 2);

}

Best Regards,

Sheng-Hua

SimonePradolini
Technical Moderator
March 3, 2023

Hi @shenghua yang​ 

The demo uses M1.

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.