Skip to main content
hkout.1
Visitor II
October 3, 2022
Question

How to enable the MLC option for the MKI197V1 in WL55?

  • October 3, 2022
  • 1 reply
  • 592 views

Hello,

I'm trying to enable the MLC option for the MKI197V1 and I'm having some trouble.

The DatalogFusion runs fine when configured for the WL55JC, but what I want is the MLC option that can be seen on the DataLogExtended sample.

Any guidance is appreciated.

    This topic has been closed for replies.

    1 reply

    ST Employee
    October 10, 2022

    I think there are a few options but unfortunately none of them is quick and easy.

    Option 1: Manually port DatalogExtended firmware which is available in X-CUBE-MEMS1 package to your board with WL55JC.

    Option 2: Create your own firmware based on PID driver for LSM6DSOX which you can find here.

    Option 3: Generate DatalogTerminal firmware using STM32CubeMX and X-CUBE-MEMS1 package and then add code working with MLC.