Skip to main content
Associate II
January 16, 2024
Question

How to store/resotre calibration data?

  • January 16, 2024
  • 2 replies
  • 1106 views

I'm using lsm6dsv, and must calibrate IMU everytime after power on. Can I read calibration data once, and restore to IMU without calibration?

This topic has been closed for replies.

2 replies

Federica Bossi
Technical Moderator
January 16, 2024

Hi @Yansu ,

Welcome to ST Community!

The IMU is calibrated at production level, and the calibration values are stored in the reserved registers, and it is better to not modify them.

However, if you need a recalibration, for example after the soldering process, you can measure the offset on the 3 axis in a steady position and write the measured values in the registers 73h-74h-75h (X_OFS_USR,Y_OFS_USR,Z_OFS_USR)

In alternative, if you have LSM6DSV16X you can use a calibration library, for example from the X-CUBE-MEMS1 package, such as the MotionAC or MotionGC: they provide real-time data calibration through offset and scale factor coefficients used to correct accelerometer and gyroscope data.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Federica Bossi
Technical Moderator
February 1, 2024

Hi @Yansu ,

Did I answer to your question?

If yes, remember to flag it as "accept as solution" to help other users :)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.