Skip to main content
Associate II
July 8, 2024
Solved

I can't use MEMS-studio under KDE/Plasma (linux)

  • July 8, 2024
  • 1 reply
  • 1429 views

Hello,

in KDE/plasma environment I can't use MEMS-studio because it doesn't show file dialogs.

For example: MEMS-studio is connected to the STEVAL-MKI109V3 board, in "Advanced Features" -> "FSM" I click the "Load state machine from file“ button, but nothing happens, the file dialog does not appear.

Is there any solution to allow MEMS-studio to work properly in the KDE/plasma environment?

When I run MEMS-studio from the command line I get this output from the console:

 

Searching in: "/home/senbuvis/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/home/senbuvis/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/home/senbuvis/STMicroelectronics/STM32Cube/bin"
Searching in: "/home/senbuvis/STMicroelectronics/bin"
Searching in: "/opt/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/opt/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/opt/STMicroelectronics/STM32Cube/bin"
Searching in: "/opt/STMicroelectronics/bin"
Searching in: "/usr/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/usr/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/usr/STMicroelectronics/STM32Cube/bin"
Searching in: "/usr/STMicroelectronics/bin"
Searching in: "/usr/local/STMicroelectronics/STM32Cube/STM32CubeProgrammer/bin"
Searching in: "/usr/local/STMicroelectronics/STM32CubeProgrammer/bin"
Searching in: "/usr/local/STMicroelectronics/STM32Cube/bin"
Searching in: "/usr/local/STMicroelectronics/bin"
Searching in: "/home/senbuvis/ST/STEdgeAI/1.0/Utilities/linux"
Searching in: "/opt/ST/STEdgeAI/1.0/Utilities/linux"
Searching in: "/usr/ST/STEdgeAI/1.0/Utilities/linux"
Searching in: "/usr/local/ST/STEdgeAI/1.0/Utilities/linux"
void DeviceManagerInterface::setIsBusy(bool) false false
void AfsManager::initParamsToDefault()
file:///home/senbuvis/Poligonas/MEMSstudio_1.3.0/opt/mems-studio/qml/QtQuick/Dialogs/DefaultFileDialog.qml:413:17: QML ToolButton: Binding loop detected for property "implicitHeight"
file:///home/senbuvis/Poligonas/MEMSstudio_1.3.0/opt/mems-studio/qml/QtQuick/Dialogs/DefaultFileDialog.qml:309:21: QML Button: Binding loop detected for property "implicitHeight"
file:///home/senbuvis/Poligonas/MEMSstudio_1.3.0/opt/mems-studio/qml/QtQuick/Dialogs/DefaultFileDialog.qml:309:21: QML Button: Binding loop detected for property "implicitHeight"
qml: OS DETECTED: linux
plugin.communication: 
app.monitoringDataModel: 
mems-studio Started, processing run parameters..

 

I'm using MEMS-studio v1.3.0.

My system specs:

 

Operating System: Arch Linux
KDE Plasma Version: 6.1.1
KDE Frameworks Version: 6.3.0
Qt Version: 6.7.2
Kernel Version: 6.6.36-1-lts (64-bit)
Graphics Platform: X11
Processors: 16 × AMD Ryzen 7 1700X Eight-Core Processor
Memory: 62.7 GiB of RAM
Graphics Processor: NVIDIA GeForce GTX 1080 Ti/PCIe/SSE2

 

 

 

 

 

Best answer by Federica Bossi

Hi @zmogas ,

Welcome to ST Community!

Thank you for using MEMS Studio, we are sorry you are facing some issues. MEMS Studio is officially supported on Ubuntu Linux 20.04 or higher however it shall also run on Arch Linux.

File dialogs should work correctly when application is started using provided mems-studio.desktop file. If this is not the case, you can start the application from console using this command:

QT_QPA_PLATFORMTHEME=gtk3 QT_QPA_PLATFORM=xcb /opt/mems-studio/bin/mems-studio

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
July 9, 2024

Hi @zmogas ,

Welcome to ST Community!

Thank you for using MEMS Studio, we are sorry you are facing some issues. MEMS Studio is officially supported on Ubuntu Linux 20.04 or higher however it shall also run on Arch Linux.

File dialogs should work correctly when application is started using provided mems-studio.desktop file. If this is not the case, you can start the application from console using this command:

QT_QPA_PLATFORMTHEME=gtk3 QT_QPA_PLATFORM=xcb /opt/mems-studio/bin/mems-studio

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
zmogasAuthor
Associate II
July 9, 2024

It works, thanks!

Yes, I tried running the mems-studio.desktop file, but the file dialogs didn't show up either.

The exported variable "QT_QPA_PLATFORM=xcb" fixed the problem with file dialogs.

But I found it strange that MEMS-studio (which uses Qt libraries) does not work out of the box in Qt-based KDE/plasma environment, but it works correctly in Ubuntu, where the graphical environment is GTK...