Skip to main content
Associate
July 11, 2024
Question

I have a problem of power down of ASM330LHH

  • July 11, 2024
  • 3 replies
  • 1939 views

As you can see, I was doing a test where I tried setting the gyroscope and accelerometer to power down mode and gave it a 10ms delay, which I called time 1, while I again turned the gyroscope on The accelerometer is set to high-performance mode, and a 70ms delay is given to the data again. This time is called time 2. After exiting, I start reading the data. At this time, the data is read normally after leaving this code, but between time 1 and time After the time of 2 is changed (only the time becomes shorter), the read data will have data errors for a long time. I would like to ask you for some advice. At the same time, time 1 and time 2 are 300us and 70ms respectively in the manual. Want to know why there is such a big discrepancy? Below is my code. Thanks,

 

 

2.png

3 replies

Associate
July 11, 2024

代码图片代码图片

The unit of delay_us is 2us

TDK
Super User
July 11, 2024

No pictures or code came through. You can edit your post using the down arrow at the top-right of the post.

TDK_0-1720712189699.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
July 11, 2024

thank you ! This is my first time posting。

屏幕截图 2024-07-11 233457.png

this is my code , The unit of delay_us is 2us,comment have some error ,sorry ! wish you can understand it.

Associate
July 11, 2024

sorry,comment have some error,wish you can understand it ! thank you!!!