Skip to main content
Associate
April 17, 2024
Solved

IIS3DWB - ODR Accuracy

  • April 17, 2024
  • 1 reply
  • 1351 views

Hello,
I am working with the IIS3DWB for a vibration monitoring sensor, and have a few questions about the ODR (Output Data Rate) accuracy, hoping someone can help me.

1. I know that on the datasheet the ODR accuracy is stated as +-1% typ, or +-2% Max.
I want to know, does this accuracy specification include using the INTERNAL_FREQ_FINE register to correct the ODR (See page 45)? If we use the contents of that register is the tolerance considered more accurate?

2. I am also curious if anyone knows the INTERNAL_FREQ_FINE register is set once in manufacture, or if the contents change over time. Should I read this register once or read it regularly to update my data rate correction.
2.a. I know there is also a characteristic to describe the ODR change with respect to temperature. Is this characteristic captured in the adjustment provided by the INTERNAL_FREQ_FINE register? Or would it be beneficial for me to apply this correction in post processing?

Thank you in advance to anyone who can help me with this or point me to more resources!

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @Wellett ,

Welcome to ST Community!

1. No, the INTERNAL_FREQ_FINE reg was not enabled. If you use it, the accuracy will improve.

2. It is set once in manufacture.

3. With the INTERNAL_FREQ_FINE register you will improve the value at 25DegC

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
April 18, 2024

Hi @Wellett ,

Welcome to ST Community!

1. No, the INTERNAL_FREQ_FINE reg was not enabled. If you use it, the accuracy will improve.

2. It is set once in manufacture.

3. With the INTERNAL_FREQ_FINE register you will improve the value at 25DegC

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
WellettAuthor
Associate
April 19, 2024

Thank you for the fast response, it is very helpful!

Thanks,
William