IIS3DWB - Registers reset with STEVAL-MKI208V1K
Hello,
I have a setup with a processing unit connected to two IMU sensors via SPI.
One of those IMU's is the IIS3DWB.
I am configuring the IIS3DWB with FIFO in continuous mode and I can read data properly from FIFO.
I decided to make long run tests. With these tests, I noticed that some times after 10 minutes, after 2h or more, I can't read data from the IIS3DWB FIFO since the values read from FIFO_STATUS1 and FIFO_STATUS2 are 0.
I wrote a piece of code to only run after this transition from proper read to read 0's, where I read the CHIP_ID and the FIFO_CTRL registers. The result is a proper read of the CHIP_ID and the all FIFO_CTRL registers are read as 0.
It looks to me that some reset occurred to the internal registers. Aren't the capacitors of the STEVAL board making his job?
As a note, the other IMU continuous working properly and SPI bus also does not present any issue.
Do you have a suggestion on how to mitigate or debug further?
Thank you.