Skip to main content
KMeld.1
Associate III
June 30, 2022
Question

IIS3DWB uses ~275uA in Low power mode - not 5uA-16uA

  • June 30, 2022
  • 2 replies
  • 2246 views

I have an issue with current consumption of a IIS3DWB using the STEVAL-MKI208V1 kit.

I have previously discussed it in this issue, but I've traced (i hope) the issue to the VDDIO pin.

I'm using a STM32WB55CEU6 as SPI master.

To measure current I'm using the X-Nucleo-LPM01A.

When the ISS3DWB is in low-power mode it should use 5-16uA, but I'm measuring ~265uA.

Schematic:

0693W00000QKYsGQAX.jpg0693W00000QKYsLQAX.jpg 

Measurement of ONLY the STEVAL-kit VDD-pin (ISS3DWB in Low-power - VDDIO pin connected to MCU VDD):

0693W00000QKYsBQAX.jpg 

Measurement of the STEVAL-kit VDDIO-pin (ISS3DWB in Low-power - VDD pin connected to MCU VDD):

0693W00000Nt7M1QAJ.pngMeasurement of STEVAL-kit VDD + VDDIO in low-power-mode

0693W00000Nt7NdQAJ.png 

I'm not sure I understand why VDDIO is drawing so much current - isn't it supposed to be the SPI voltage reference?

Any ideas?

Regards

This topic has been closed for replies.

2 replies

Eleon BORLINI
ST Employee
July 5, 2022

Hi @KMeld.1​ ,

which Vdd level are you using?

Please consider that a general suggestion is to keep the VddIO level equal or below the Vdd level.

And note that the VddIO will draw the current generated by the commutation of the dataout drivers during SPI communication.

-Eleon

Associate II
July 13, 2023

We have set the register "write [000] to XL_EN[2:0} in CTRL1_XL(0x10)" and SPI(MOSI,MISO,CLK),INT1,INT2 are low voltage at sleep mode but still the current consumption is 0.28mA.Please let us know the exact pin configurations(Pull,Mode,Value) to be done at MCU(STM32L562) in sleep mode.

KMeld.1
KMeld.1Author
Associate III
July 6, 2022

Hi @Eleon BORLINI​ 

Vdd is 3.3V across the whole system. VddIO is connected to this *** well. Only for the "pure" VddIO meassurement was it isolated on the X-Nucleo-LPM01A meassurement pin.

I can see now that one grapch wasn't included in the original post - please see edit.

i can definately tolerate current consumption of the SPI suring communication and sampling, but what bothers me is the current draw AFTER I put the IIS3 into "low-power-mode" and deinit the SPI on MC (2nd graph).

Couldi t be releated to the 33Ohm resisters on the STEVAL-kit?

regards.