Skip to main content
fz_gabriel
Associate
September 3, 2024
Question

ILPS28QSW return incorrect values after transitioning between AH modes.

  • September 3, 2024
  • 0 replies
  • 538 views
Hi,

I'm working on a driver for the ST ILPS28QSW.
When I switch from Pressure to Qvar mode (using the CTRL_REG3.AH_QVAR_EN bit), I notice a brief transition problem: The first 3 samples read are invalid.
 
fz_gabriel_0-1725390060047.png

 

 


 
Please note that those incorrect samples are measured only when the STATUS.P_DA bit is set (therefore new pressure data should be generated).

Is there a way to know when the data is stable?
Is there a way to change between pressure and Qvar mode without reading those invalid samples?


Regards,
Gabriel