Skip to main content
Associate
January 13, 2025
Question

iNemoEngin/fusion sensors in stm-sensors-hal-iio for Android

  • January 13, 2025
  • 1 reply
  • 575 views

I am looking for information about iNemoEngine sensors in the latest STMicroelectronics HAL for Android.
I successfully integrated the STMicroelectronics HAL framework into Android 11. I am using the LSM6DSOTR gyroscope/accelerometer and the LIS3MDLTR magnetometer. These sensors are correctly detected and can be accessed from an Android application. However, the STMicroelectronics HAL also creates iNemoEngine sensors, which do not return any values.
The previous STMems_Android_Sensor_HAL_IIO framework used several proprietary STM libraries, including SENSOR_FUSION, GEOMAG_FUSION, GBIAS, MAGCALIB, and ACC_CALIB, to generate the game_rotation_vector, orientation, and rotation_vector sensors. Are these libraries still required for the latest STMicroelectronics HAL framework? What is needed to gain access to these libraries?
What is required to make the fusion sensors work in the latest STMems_Android_Sensor_HAL_IIO?

1 reply

Federica Bossi
Technical Moderator
January 17, 2025

Hi @zmb2024 ,

iNemoEngine sensors are composite sensors and require the installation of some STMicroelectronics proprietary libraries. If these libraries are not installed, iNemoEngine sensors exported from SensorHAL return null values, however composite sensors implemented in the Android sensor framework (AOSP) can be used instead.
The release of STM proprietary libraries is subject to signature of a License User Agreement (LUA); please contact the online support here for further information.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
zmb2024Author
Associate
November 6, 2025

Hello Federica,

I have gained access to the STM proprietary libraries and was able to integrate them into Android 11. The HAL works as expected; all sensors are available, including the composite sensors.
I have one question about sensor calibration. The STM sensors HAL framework looks for calibration data in the following files:
accel_bias<module_id>.dat
gyro_bias_<module_id>.dat
magn_bias_<module_id>.dat
What is the format of these files? How can I generate the calibration data? Is there an Android application or sample code available for calibration? Additionally, is there any documentation available on these processes?