Skip to main content
Visitor II
November 14, 2025
Solved

ISM330BX datasheet error. In AN6109 (device application note)

  • November 14, 2025
  • 1 reply
  • 156 views

anyone know who to contact about an error in the datasheets?

 

In the AN6109 (device application note) of the ISM330BX datasheet on page 65/107 in section 8.2 FIFO registers there are three line I believe have errors:

 

– SFLP_GBIAS_FIFO_EN bit of the EMB_FUNC_FIFO_EN_B register in order to enable batching the gyroscope bias data in FIFO (the SFLP embedded function must be enabled)

– SFLP_GRAVITY_FIFO_EN bit of the EMB_FUNC_FIFO_EN_B register in order to enable batching the gravity vector data in FIFO (the SFLP embedded function must be enabled)

– SFLP_GAME_FIFO_EN bit of the EMB_FUNC_FIFO_EN_B register in order to enable batching the game rotation vector data in FIFO (the SFLP embedded function must be enabled)

 

 

these three lines should say EMB_FUNC_FIFO_EN_A register not EMB_FUNC_FIFO_EN_B register.

 

 

also, and this part I'm less sure about, on the same document on page 57/107 in section 6.5 Sensor fusion functions I think the "the specific configuration below must be applied after the device boot" specifically this line:

 

4. Write D2h to PAGE_ADDRESS

 

either it shouldn't be D2h or I am just brain farting and misreading the "Table 5. Embedded advanced features registers - page 1" section

 

Thanks.

 

Best answer by Federica Bossi

Hi @no_it ,

Thank you for bringing this to our attention. I will ask the team to check and correct it if necessary.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
November 20, 2025

Hi @no_it ,

Thank you for bringing this to our attention. I will ask the team to check and correct it if necessary.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.