ISM330DHCX temperature reading?
Hello,
We have the ISM330DHCX designed into a new product but I am having trouble getting reliable readings using the I2C interface. I am able to read the WHOAMI register and get 0x6B but OUT_TEMP_L (20h), OUT_TEMP_H (21h) always return zero.
I have the interface instrumented and I can see that the signalling is correct, with repeated start and everything, but only zeros.
Does anyone have a suggestion of how this is happening? Do I need to do something special to enable temperature readings?
Thanks