Skip to main content
ECiot.1
Associate II
May 4, 2023
Question

Library/function to acquire QVAR data from the sensor LSM6DSV16X

  • May 4, 2023
  • 1 reply
  • 992 views

Hi, I would like to know if there are a library and a function to acquire QVAR data from the ST sensor LSM6DSV16X as for example it is present for the ILPS22QS sensor for Arduino using a Nucleo-64 stm32 board.

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    Technical Moderator
    May 5, 2023

    Hi @ECiot.1​,

    There isn't a library only for Qvar sensor but you can refer to the Application Note AN5755.

    In section 4.2, there is the register configuration for LSM6DSV16X to enable the Qvar sensor and how to read the results.


    _legacyfs_online_stmicro_images_0693W00000bjSX6QAM.pngIf my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster :)

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.