Skip to main content
Associate III
February 7, 2024
Solved

LIS2DH12 accelerometer SPI Interface Clock Speed

  • February 7, 2024
  • 1 reply
  • 1107 views

Hello,

 

What is the maximum data transfer rate over the SPI interface for the LIS2DH12 accelometer? The datasheet doesn't say anything about this. About the I2C interface it is said that it can operate in standard mode (up to 100 kHz) and fast mode (up to 400 kHz). But nothing is said about the SPI interface.

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @MykolaLevun ,

Please refer to page 13 of the datasheet:

FedericaBossi_1-1707306380982.png

 

 

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
February 7, 2024

Hi @MykolaLevun ,

Please refer to page 13 of the datasheet:

FedericaBossi_1-1707306380982.png

 

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate III
February 7, 2024

Thank you!