[LIS2DUXS12] FIFO: one xyz sample lost every each 1055 samples
Hi,
I'm using the LIS2DUXS12 in FIFO Stream mode with DEC_TS_32. FIFO watermark is set to 64. Looks like every ~17 FIFO reads (~1055 XL samples), exactly 1 accelerometer sample is lost. The pattern is consistent and repeatable.
Each FIFO read of 64 entries normally contains 62 XL samples + 2 timestamp tags. However, every 17th read contains 63 XL + 1 timestamp tag. Looks like before this batch with 63 XL samples, there is 1 XL sample gap in data.
I use only the timestamp present in the FIFO batch to calculate timestamp for each sample. And with that approach samples in that FIFO batch aligns with next FIFO batch exactly - no gaps, no overwriting, fixed period.
So despite the fact that this FIFO batch contains one XL sample more than the other, there's still a gap in data.
Configuration:
- ODR: 200 Hz (HP mode)
- FIFO mode: Stream (continuous)
- bdr_xl: ODR
- dec_ts: DEC_TS_32
- xl_only_fifo: 1
- FIFO watermark: 64
I couldn't find errata for LIS2DUXS12.
Questions:
1. Is this a known hardware behavior — does the TS tag replace (instead of accompany) the triggering XL sample at certain FIFO alignment boundaries?
2. Is there a recommended workaround?