Skip to main content
Associate
March 18, 2024
Question

LIS2MDL - impact to ODR When Set_FREQ = 1

  • March 18, 2024
  • 1 reply
  • 731 views

Hi 

 

Can someone clarify how long it takes for the sensor to temporarily stop reading, execute the SET pulse, and begin conversion when Set_FREQ is set to 1 in CFG_REG_B (61h) while in continuous conversion mode?

 

I noticed that this setting randomly changes my ODR rate. 

 

Thank you.

 

This topic has been closed for replies.

1 reply

Federica Bossi
Technical Moderator
March 19, 2024

Hi @Indi ,

Which difference in the ODR rate did you notice?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.