Skip to main content
Dillah
Associate II
October 31, 2019
Solved

LIS3DH Single/Double Tap Detection Current Consumption

  • October 31, 2019
  • 5 replies
  • 3507 views

Hi,

We notice that LIS3DH accelerometer has multiple mode which can be utilized to be used on low power mode for single/double tap detection.

Does single/double tap detection increase the current consumption stated on the data sheet/design tip?

https://www.st.com/resource/en/datasheet/lis3dh.pdf

https://my.st.com/content/ccc/resource/technical/document/design_tip/group0/d6/1d/5f/b0/3c/6e/47/27/DM00564061/files/DM00564061.pdf/jcr:content/translations/en.DM00564061.pdf

Thank You

    This topic has been closed for replies.
    Best answer by Eleon BORLINI

    Hi @Dillah​ , sorry for my delayed answer. From the LIS3DH app note AN3308 (p. 31), the recommended accelerometer ODR for single and double-click recognition is 400 Hz or higher. You can however try to lower this ODR and check if the feature is working in your specific application case, if the low current consumption is a major request. Or you could try with a more recent sensor like the LIS2DW12 to get lower power consumption on double tap application. Regards

    5 replies

    Eleon BORLINI
    ST Employee
    November 4, 2019

    Hi @Dillah​ , the typical current consumption contribution of a digital embedded feature such as the single/double tap detection (that includes a couple of threshold comparisons) is less than 1uA, a fraction of the overall standard current consumption. Regards

    Dillah
    DillahAuthor
    Associate II
    November 5, 2019

    HI Borlini,

    Thanks for the information.

    Is there any recommendation on minimum data rates for acceptable double tap performance?

    Noted that tap threshold will be acquired by manual testing on the unit.

    We want to use as low current consumption as possible.

    Eleon BORLINI
    Eleon BORLINIBest answer
    ST Employee
    November 25, 2019

    Hi @Dillah​ , sorry for my delayed answer. From the LIS3DH app note AN3308 (p. 31), the recommended accelerometer ODR for single and double-click recognition is 400 Hz or higher. You can however try to lower this ODR and check if the feature is working in your specific application case, if the low current consumption is a major request. Or you could try with a more recent sensor like the LIS2DW12 to get lower power consumption on double tap application. Regards

    Dillah
    DillahAuthor
    Associate II
    January 28, 2020

    Hi @Eleon BORLINI​ .

    Currently we are working in 3V environment, and we are computing power budget.

    However we can not find LIS2DW12 averaged current consumption on 3V voltage supply.

    I would ask if you have similar data to current consumption vs voltage supply?

    Thanks

    Dillah
    DillahAuthor
    Associate II
    January 29, 2020

    Hi @Eleon BORLINI​ ,

    Thank you for those information.

    Our power budget on accelerometer is around 3uA in 3V supply voltage.

    After some evaluation, we will try to use 25Hz or 50Hz ODR as shown on below image.0690X00000BwmISQAZ.pngI would ask if you have similar data of current consumption in 3V power supply for highlighted mode?

    Thanks

    Eleon BORLINI
    ST Employee
    January 29, 2020

    @Dillah​, of course going in LPM will help the power budget requirements. The curr cons for 3V in LP1 at that ODRs is about 2.5uA with ODR 25Hz, so this is the condition in your case. Please note that the resolution lowers from 14-bit to 12-bit, you should have to check if you can detect the single/double tap in a good way. Regards

    Dillah
    DillahAuthor
    Associate II
    January 29, 2020

    HI @Eleon BORLINI​ ,

    Thanks for the info.

    We will try to test the double/single tap sensitivity of said setting.

    GGabi.1
    Associate
    February 12, 2024

    Hi @Dillah,

     

    Did you have the opportunity to test the current consumption putting the sensor in low power mode? 

    If so, what was the averaged result?

     

    Reading from the datasheet I'm afraid that sensing single/double tap is only possible running the sensor in high performance mode.

     

    Thanks in advance,

    Dillah
    DillahAuthor
    Associate II
    February 13, 2024

    Hi @GGabi.1,

    The current consumption are consistent with what it shows in the datasheet.

    Our development was limited by current consumption limitation, so i only used the lower ODR rates to keep the current below 5uA on average.

     

    Thank You.

    GGabi.1
    Associate
    February 13, 2024

    Thanks @Dillah for your fast answer

     

    So, are you telling me that you did successfully the tap detection implementation with an average of current consumption of only 5uA? And it worked well?

    I guess that as you cannot set the wake-up interrupt of tap detection in low power mode, then you have needed to use a fixed threshold to wake-up and then change the operative mode of the sensor to active mode, changing the ODR sampling rate. 

    Is my assumption correct?

     

    Thanks in advance