Skip to main content
Associate III
March 19, 2025
Solved

LPS22HB Absolute pressure accuracy

  • March 19, 2025
  • 1 reply
  • 443 views

Hello,

in the datasheet of LPS22HBTR the absolute pressure accuracy is between 0. and 1 mBar in the range of 0°C and 65°C .

Please have more information about the absolute pressure accuracy in negative temperature ? because i will use it betwen -20°C and 0°C

thanks 

Best answer by Federica Bossi

Hi @ljm ,

We can't provide this type of information on ST Community.

If you need data in the negative temperature range you should contact your FAE of reference or the Online Support System at this link.

1 reply

Federica Bossi
Federica BossiBest answer
Technical Moderator
March 21, 2025

Hi @ljm ,

We can't provide this type of information on ST Community.

If you need data in the negative temperature range you should contact your FAE of reference or the Online Support System at this link.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.