Skip to main content
DGand.2
Visitor II
May 7, 2023
Question

LPS22HB gives inconsistent readings

  • May 7, 2023
  • 1 reply
  • 938 views

Please refer this thread. I don't think that the sensor can get damaged in such short period of time. Is it possibly due to moisture? At times I get 1018hPa which is even higher than sea level pressure of 1013.5 hPa

Pls help.

    This topic has been closed for replies.

    1 reply

    Federica Bossi
    Technical Moderator
    May 17, 2023

    Hi @DGand.2​ ,

    Welcome to ST Community!

    On pressure sensors there are very small holes on the silicon exposed cap area of the package to allow external pressure to reach the sensing element and for this reason they should be kept clear of obstructions, in particular humidity can affect the measures.

    If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster :)

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.