Skip to main content
hmckee
Associate
March 26, 2025
Question

LPS22HH temperature readings

  • March 26, 2025
  • 1 reply
  • 385 views

Anyone have any idea if the temperature can remain the same for long periods of time in a stable environment?

1 reply

Federica Bossi
Technical Moderator
March 27, 2025

Hi @hmckee ,

It should. Did you try?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
hmckee
hmckeeAuthor
Associate
March 27, 2025

Yes, that's the issue. We've set up our device so that it marks the LPS22 in error if it reads the same value 45 times in a 30 min period. The condition has occurred in both a stable, temperature controlled environment and in an uncontrolled environment.

The purpose of this was to determine if the LPS22 is functioning properly. Maybe this is an unrealistic expectation.