Skip to main content
Associate
August 6, 2023
Question

LPS28DFW bias stability / difference with other LPS28DFW

  • August 6, 2023
  • 2 replies
  • 1355 views

Hi,

I have two LPS28DFW in my application. The absolute value as well as the difference is important here. I noticed that there is a difference of around 30 Pa. Is it reasonable to assume that this difference is roughly constant in the future? I tested it for around 5000 seconds (see attached scatter plot and histogram for the difference) and it was pretty stable (sensor temperature was ~31°C in both cases). I am also going to test it for a longer time period but I'd like to know from a theoretical standpoint if I can assume this to be roughly constant and if I can use this for a "factory calibration" of my application to improve accuracy.

Thanks for your help.

This topic has been closed for replies.

2 replies

TDK
Super User
August 6, 2023

Per the data sheet, the devices are factory calibrated, so if they're registering 30 Pa off, that means the reading has changed between factory calibration and now.

The datasheet specifies ± 50 Pa difference from soldering, which is in line with what you're seeing, and ± 100 Pa drift per year. These are specified as "typical" values, not max, so that's roughly how you should expect them to perform long term.

TDK_0-1691333694455.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate
August 6, 2023

Thanks for the information. Is there some recommended calibration procedure which I can implement to improve accuracy? Is it just the offset/bias or is a more complicated temperature dependent calibration necessary? In any case how does a function look like which applies calibration parameters?