Skip to main content
Associate III
March 18, 2024
Solved

LPSS22DF accuracy between -15°C and 60°C

  • March 18, 2024
  • 2 replies
  • 5146 views

Hi

I'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is  ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the range -15 to 65°C?

This topic has been closed for replies.
Best answer by Federica Bossi

Hi @ljm ,

We tested few parts and I confirm you that the accuracy was around 2°C but consider that we considered a limited number of pcs and thus this value can't be guaranteed in production.

2 replies

AScha.3
Super User
March 18, 2024

Hi,

pressure - from ds:

AScha3_0-1710748297889.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
ljmAuthor
Associate III
March 18, 2024

hello @AScha.3 

thanks for replying.

I'm speaking about the temperature accuracy.. in the datasheet it is  ±1.5 °C (T = 0 to 80°C), but my working range is betwwen -15°C   and +60°C... just if it's possible i want to know the accuracy is the same between -15°C and 0°C or h

greater than the accuracy betwwen 0°C and 80°C ?

Thank you in advance

 

 

taccuracy.png

AScha.3
Super User
March 18, 2024

>if it's possible i want to know the accuracy

Its not specified, so test it yourself, to know for sure.

Anyway at +/-1,5°  this is more guessing "temp. is about" , so if you want measure temperature, take a temperature sensor to do this (and not a pressure sensor).

I use the ENS210 , temp. + humidity :

AScha3_0-1710752403123.png

 

Or a pressure + temperature sensor, like BMP280 (or BME280 etc. ); this can with some interpolation give a temperature resolution of 1/1000 ° !  (I tried, is funny, you can see when your go to the table, the bmp280 is there, temperature rising about 0,003° - from body IR radiation ! )

"If you feel a post has answered your question, please click ""Accept as Solution""."
Federica Bossi
Federica BossiBest answer
Technical Moderator
April 4, 2024

Hi @ljm ,

We tested few parts and I confirm you that the accuracy was around 2°C but consider that we considered a limited number of pcs and thus this value can't be guaranteed in production.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.