Skip to main content
CSharpino
Associate II
May 26, 2023
Question

lsm303agr power-down current consumption?

  • May 26, 2023
  • 3 replies
  • 1853 views

I have several lsm303agr that with the accelerometer and the magnetometer in power-down mode consume between 40uA and 20uA while others consume about 2uA as indicated on the datasheet.

Even if they have this higher consumption, they perform the self tests correctly.

What could this behavior be caused by?

In my board Vdd = VddIO = 3V

    This topic has been closed for replies.

    3 replies

    Federica Bossi
    Technical Moderator
    May 26, 2023

    Hi @CSharpino​,

    As specified in the datasheet the typical value of 2uA is measured when Vdd=2.5V and with a temperature of 25 °C.

    Can you retest the parts that consume 40uA or 20uA under these conditions and let me know if this extra consume is already present?

    Thanks

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    CSharpino
    CSharpinoAuthor
    Associate II
    May 26, 2023

    I tried with a 2.5V supply voltage, consumption drops but always remains between 30uA and 15uA.

    Federica Bossi
    Technical Moderator
    May 26, 2023

    Ok, can you share your board's schematic?

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
    CSharpino
    CSharpinoAuthor
    Associate II
    May 29, 2023

    This is the schematic. Don't pay attention to the fact that IIS2MDC is written there because the board provides the possibility to mount this component too.

    The power is supplied through the Mosfet Q4 to have the possibility to completely switch off the component when not in use.

    To put the device into power-down mode using these calls to the ST driver:

    	lsm303agr_mag_operating_mode_set(&mag_ctx, LSM303AGR_POWER_DOWN);
    	lsm303agr_mag_power_mode_set(&mag_ctx, LSM303AGR_LOW_POWER);
    	lsm303agr_xl_data_rate_set(&xl_ctx, LSM303AGR_XL_POWER_DOWN);


    _legacyfs_online_stmicro_images_0693W00000bl1ynQAA.png

    Federica Bossi
    Technical Moderator
    June 1, 2023

    Hi @CSharpino​ ,

    The schematic seems ok, what you could try is to reverse commands like this:

    • lsm303agr_xl_data_rate_set(&xl_ctx, LSM303AGR_XL_POWER_DOWN);
    • lsm303agr_mag_power_mode_set(&mag_ctx, LSM303AGR_LOW_POWER);
    • lsm303agr_mag_operating_mode_set(&mag_ctx, LSM303AGR_POWER_DOWN);

    Let me know if this helps.

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.