Skip to main content
Associate II
January 16, 2025
Solved

LSM6DS3 + LIS3MDL calibration

  • January 16, 2025
  • 4 replies
  • 1742 views

Hello, 

Our teams is making a proof of concept about dead reckoning using a STM WESU board. 

The goal is to get pedestrian position onyl using ACC/GYR/MAG for a short period of time and small moves.

First results in certains conditions are pretty good. Without any calibration/correction, we manage to get approx 3m absolute error on a 20m walk (30seconds). We expect same error on a 100m walk with good AHRS algorithm parameters and sensor calibration.

We are ready to put more effort on the IMU. 

Do you have calibration source code/protocol for WESU sensor ? 

* LSM6DS3 = acc value + gyro drift

* LIS3MDL = soft and hard iron calibration

We also have other more advanced IMU, but we want to keep it simple and low cost for now and WESU allow us to be pretty fast on POC steps.

Thanks a lot for your future help.

 

Best regards.

 

Best answer by Andrea VITALI

Forgot to mention: the latest and best evaluation platform today is SensorTile.Box PRO for the consumer market, or the STWIN.Box for industrial applications.

4 replies

Federica Bossi
Technical Moderator
January 29, 2025

Hi @pierre63 ,

 

The WeSU board is not a recent board and therefore integrates the sensors that were available when it was designed, being an integrated solution obviously there is no way to update the sensors with more current ones.


The fw package integrates a calibration routine for the magnetometer only, built into the MotionFX package. In the firmware, the reference is the MotionFX_manager_MagCal_run function.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pierre63Author
Associate II
January 29, 2025

Hello Federica, 

Thanks a lot for your reply.

Yes, this demo board is a bit old, but pretty well integrated and pretty good to make demo.

I checked this function, but there is no the source code available.

Also, for gyroscope or accelerometer, do I only need to apply offset or there is another correction to apply ?

Thanks,

Federica Bossi
Technical Moderator
January 29, 2025

Hi @pierre63 ,

For gyroscope and accelerometer we don't have any example code but yes, you can use the offset when the sensor is in a steady state position.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pierre63Author
Associate II
February 10, 2025

Hello Federica, 

Before closing the topic, I have few questions :

* Since our last discussion, we want now to focus on activity detection (walking, carrying, steady, driving) instead of raw data measurement. Could you please recommand which eval board can I use for the project ?

* We need to finish the POC and I need to add memory on the board, but I can identify test point on the PCB (Gerber file don't mention it). Could you send me the Test point location if possible ?

 

Thanks a lot,

 

Regards,

 

 

Andrea VITALI
ST Employee
February 13, 2025

MotionFX, the sensor fusion library, does include a robust version MotionMC, which is the magnetometer calibration library, but which only performs sphere fitting hence computing hard-iron to be subtracted. MotionFX also includes gyroscope bias estimation. For reference see UM2220 for MotionFX.

MotionFX is fed with raw accel and gyro data, and compensated mag data (compensated by subtracting the hard-iron coming from the embedded magnetometer calibration library).

Alternatively, one can include and run the full blown MotionMC (X-Cube-MEMS1 package) which performs ellipsoid fitting and therefore also computes the soft-iron matrix for the magnetometer compensation. This WESU software package can indeed be modified and customized by including MotionMC.

If this is done then running the mag calib embedded in MotionFX is no more necessary. MotionFX will need to be fed with compensated mag data: first subtract hard-iron, then apply the soft-iron matrix coefficients.

(for more details on mag calibration one can also check design tip DT0059)

 

 

Andrea VITALI
Andrea VITALIBest answer
ST Employee
February 13, 2025

Forgot to mention: the latest and best evaluation platform today is SensorTile.Box PRO for the consumer market, or the STWIN.Box for industrial applications.

pierre63Author
Associate II
February 13, 2025

Hello Andrea,

Thanks a lot for this informations. I checked MotionMC and that exactly what I'm looking for about magnetometer correction. 

Also, I will buy a SensorTile.Box PRO for datastream and logging instead of customize the WESU. 

I'm closing the toping and if needed I will open another one.

Regards,