Skip to main content
Visitor II
August 19, 2024
Question

LSM6DSL big gyroscope fluctuations on acceleration

  • August 19, 2024
  • 1 reply
  • 667 views

Hello,

 

I am using a LSM6DSL sensor and when applying a 2G acceleration without rotating the board, I get very important spikes on the gyroscopes of about -90°/s to +90°/s amplitude.

This is very strange. Is this a normal behaviour from this sensor ? Are there settings or ways to avoid this ?
I noticed the exact same behaviour on the LSM6DSV16X sensor.

Thank you for your help

1 reply

Federica Bossi
Technical Moderator
August 29, 2024

Hi @AnselmeC1 ,

Have you enabled the BDU bit in register CTRL3_C (12h)? If not, can you please try?

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.