Skip to main content
Associate
March 28, 2025
Question

LSM6DSO analog anti aliasing

  • March 28, 2025
  • 1 reply
  • 520 views

Hi,

I would like to confirm if setting LSM6DSO ODR to 6.66KHz and LPF2 to ODR/10 (resulting to 666Hz bandwidth), then setting a FIFO decimation factor of 8 (resulting to 833hz FIFO ODR) will work in preventing aliasing for signals above 417Hz?

 

We have discovered with LSM6DSL that it doesn't work that well, but looking at a previous post where the LSM6DSO is recommended (Solved: LSM6DSL anti-aliasing filters do not appear to be ... - STMicroelectronics Community). So I would like to confirm it before we do a hardware change in production.

 

Thank you. 

1 reply

Federica Bossi
Technical Moderator
April 4, 2025

Ciao @adrianT ,

LSM6DSO has effectively more performing filter like descripted in the other post.

Regarding your case using FIFO decimation of 8 result to a sampling frequency of 833 Hz while should be double respect signal bandwidth 2*ODR/10 = 1333 Hz. So I would suggest to use FIFO BatchDataRate of 4 to avoid aliasing.

Otherwise you can set LPF2 to have ODR/20 and leave sampling frequency with FIFO decimation of 8.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
adrianTAuthor
Associate
April 14, 2025

Thanks for the confirmation. We determined that our setup can handle at most 1660Hz without requiring major changes in FW.

 

Would there be a difference in filtering performance (specifically in LPF for anti aliasing) if for example we just run the sensor in 1660hz ODR, no FIFO decimation and rely on LPF1 (ODR/2 = 833hz bandwidth)

compared to 6.6KHz ODR, FIFO decimation factor 4, LPF2 set to ODR/10 (Resulting to 666Hz bandwidth)

 

Both bandwidths are are acceptable in this case as we only need data right up to ~500hz. Anything above should be attenuated or at least not aliased back into the 0-500Hz data.

Associate
February 23, 2026

Hi Adrian

We are facing a similar appliacation with a LSM6 vibration sensor. Our target vibration measurment range is also 0-500Hz. Despide different configuraitons we still see down-folded signal artefacts in the spectrogram from input singals > 500Hz. LPF2 does not seem to have any affect on the output data at all. 
What is your epirences? Is the LSM6 working in your application, if yes can you share your sensor configuration?

Thanks Simon