Skip to main content
Dude
Associate III
September 27, 2024
Question

LSM6DSO Register - WAKE_UP_THS - 0x5B

  • September 27, 2024
  • 1 reply
  • 667 views

Hi, 

 

I am looking at the LSM6DSO device, and I am unclear what the "USR_OFF_ON_WU" bit does in the "WAKE_UP_THS " register. Does this bit: 

  1. Drive the Wake-Up function with offset corrected accelerometer data? 0 means not offset corrected, 1 means offset corrected?
  2. What does this have to do with High-Pass Filtered Data? Does this bit actually set whether Lowpass or Highpass information is used to drive the Wakeup Function? 

 

Can someone please provide clarity? 

thanks

1 reply

Federica Bossi
Technical Moderator
October 9, 2024

Hi @Dude ,

When it is set to '1' the input data for the wake-up function comes from the low-pass filter path (instead of the high pass filtered data) and the programmable position is subtracted as an offset.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.