Skip to main content
Dude
Associate III
September 27, 2024
Question

LSM6DSO - WAKE_UP_THS - WK_THS

  • September 27, 2024
  • 1 reply
  • 724 views

Hi, 

 

  I'm looking through the LSM6DSO32X datasheet, and I'm having a hard time finding out information about certain register data bits. For instance, register "WAKE_UP_THS" (0x5b) has 6 bits labelled "WK_THS[5:0]". Are these bit signed or unsigned? I assume they are unsigned, but I would appreciate confirmation. 

 

thanks 

1 reply

Federica Bossi
Technical Moderator
October 9, 2024

Hi @Dude ,

It is an absolute value so they are neither signed nor unsigned.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.