Skip to main content
plawat
Associate III
January 16, 2023
Question

LSM6DSOX schematics verification. We are unable to detect the LSM6DSOX IC address. We used the same IC with CS as 3.3v and we could detect it. In this device we are making CS high to 3.3V via Nordic SoC pin P0-5. We checked the voltage at the Pin as

  • January 16, 2023
  • 1 reply
  • 1053 views

0693W00000Y8ERDQA3.jpg0693W00000Y8ERIQA3.jpg

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    January 18, 2023

    Hi @plawat​ ,

    are the Vdd, VddIO and CS high state (and in general the digital communication lines) all at 3.3V?

    -Eleon

    plawat
    plawatAuthor
    Associate III
    January 18, 2023

    Hi Eleon, there is 3v​ to Vdd via bead, 3v to VddIO and 3 v to CS as seen in schematics