Skip to main content
Associate II
November 27, 2025
Question

lsm6dsv calibration

  • November 27, 2025
  • 2 replies
  • 194 views

Greetings,
we are working on to evaluate the data given in lsm6dsv datasheet ,we want to verify the sensitivity and rest of the parameters,could you please provide us the test setup/suitable test rig details with which we can test the sensor...

Thank you

2 replies

Federica Bossi
Technical Moderator
November 27, 2025

Hi @shalinich67 ,

For the gyroscope, a rate table is commonly used. This device rotates the sensor at precisely controlled angular velocities, allowing you to compare the sensor output to known rotation rates. 

You can use a rate table also for the accelerometer, otherwise a tilt platform with accurately known angles is typically used to test sensitivity in static conditions. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Associate II
December 1, 2025

Hi, @Federica Bossi 
Thank you for the information.

However, rate tables and precision tilt platforms are quite expensive and beyond our budget for this evaluation. Could you please suggest a simpler or low-cost test setup that would still allow us to reasonably verify the gyroscope and accelerometer sensitivity and basic performance parameters of the LSM6DSV?

Any guidance on practical, budget-friendly test methods would be greatly appreciated.

Thank you.