Skip to main content
Associate
October 20, 2025
Solved

LSM6DSV16X External Sensor Data Logging

  • October 20, 2025
  • 2 replies
  • 232 views

Hello,

I am using an LSM6DSV16X with an external sensor on Unico-GUI. I want to train a decision that uses both the internal and external sensors as inputs for the MLC. I am trying to save data from the internal sensors as well as the external sensors, but I do not find the option to include the external sensors in the "Load/Save" in Unico-GUI, even when the LSM6DSV16X is actively reading data from the external sensor through Unico-GUI's "Sensor Hub Registers" tab. How do I use Unico-GUI to save external sensor data, and if it isn't possible, how would I include external sensor data in the training for the MLC.

 

Thank you,

Abdurrahman Farag

Best answer by Federica Bossi

Hi @Abdu ,

This feature is not currently available in Unico or MEMS Studio.

2 replies

Federica Bossi
Federica BossiBest answer
Technical Moderator
October 23, 2025

Hi @Abdu ,

This feature is not currently available in Unico or MEMS Studio.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AbduAuthor
Associate
October 26, 2025

Hello,

Thank you for your response. In the AN5804 document and LSM6DSV16X Datasheet, it mentions that MLC can use external sensor data as an input. How would I configure the LSM6DSV16X to include the external sensor data as an input? Would it require only that I include the sensor data in the training input? Please advise.

Thank you,

Abdurrahman Farag