Skip to main content
Associate II
September 16, 2024
Solved

LSM6DSV16X QVar data with XL/G/SFLP FIFO

  • September 16, 2024
  • 1 reply
  • 1242 views

Hi, in my application I intend to use the LSM6DSV16X in order to store accelerometer, gyroscope, SFLP and QVar data, all at the same time.
I am able to get XL, G and SFLP data from the FIFO on INT1 correctly, and now I want to also record QVar data.
Based off of the example provided here: https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dsv16x_STdC/examples/lsm6dsv16x_qvar_read_data_polling.c , I was able to get QVar data alone by routing it to the INT2 pin, however when I also enable the FIFO, I don't receive the data ready interrupts anymore.
Is there an incompatibility between these functions that I missed by reading the datasheet ?

 

Here is the code that I am using to set up the sensor (the commented out section are the commands that prevent QVar data from getting output):

int lsm6dsv16x_start_acquisition(bool enable_gbias)
{
	lsm6dsv16x_pin_int_route_t pin1_int;
	lsm6dsv16x_pin_int_route_t pin2_int;
	lsm6dsv16x_fifo_sflp_raw_t fifo_sflp;
	lsm6dsv16x_filt_settling_mask_t filt_settling_mask;
	int ret;

	/* Enable Block Data Update */
	ret = lsm6dsv16x_block_data_update_set(&sensor.dev_ctx, PROPERTY_ENABLE);
	if (ret) {
		LOG_ERR("lsm6dsv16x_block_data_update_set (%i)", ret);
	}
	/* Set full scale */
	ret = lsm6dsv16x_xl_full_scale_set(&sensor.dev_ctx, LSM6DSV16X_2g);
	if (ret) {
		LOG_ERR("lsm6dsv16x_xl_full_scale_set (%i)", ret);
	}
	ret = lsm6dsv16x_gy_full_scale_set(&sensor.dev_ctx, LSM6DSV16X_2000dps);
	if (ret) {
		LOG_ERR("lsm6dsv16x_gy_full_scale_set (%i)", ret);
	}

	/*
	* Set FIFO watermark (number of unread sensor data TAG + 6 bytes
	* stored in FIFO) to FIFO_WATERMARK samples
	*/
	ret = lsm6dsv16x_fifo_watermark_set(&sensor.dev_ctx, FIFO_WATERMARK);
	if (ret) {
		LOG_ERR("lsm6dsv16x_fifo_watermark_set (%i)", ret);
	}

	/* Set FIFO batch XL/Gyro ODR to 60Hz */
	ret = lsm6dsv16x_fifo_xl_batch_set(&sensor.dev_ctx, LSM6DSV16X_XL_BATCHED_AT_60Hz);
	if (ret) {
		LOG_ERR("lsm6dsv16x_fifo_xl_batch_set (%i)", ret);
	}
	ret = lsm6dsv16x_fifo_gy_batch_set(&sensor.dev_ctx, LSM6DSV16X_GY_BATCHED_AT_60Hz);
	if (ret) {
		LOG_ERR("lsm6dsv16x_fifo_gy_batch_set (%i)", ret);
	}

	/* Set FIFO mode to Stream mode (aka Continuous Mode) */
/*
	ret = lsm6dsv16x_fifo_mode_set(&sensor.dev_ctx, LSM6DSV16X_STREAM_MODE);
	if (ret) {
		LOG_ERR("lsm6dsv16x_fifo_mode_set (%i)", ret);
	}

	pin1_int.fifo_th = PROPERTY_ENABLE;
	ret = lsm6dsv16x_pin_int1_route_set(&sensor.dev_ctx, &pin1_int);
	if (ret) {
		LOG_ERR("lsm6dsv16x_pin_int1_route_set (%i)", ret);
	}
*/
	/* Set Output Data Rate */
	ret = lsm6dsv16x_xl_data_rate_set(&sensor.dev_ctx, LSM6DSV16X_ODR_AT_960Hz);
	if (ret) {
		LOG_ERR("lsm6dsv16x_xl_data_rate_set (%i)", ret);
	}
	ret = lsm6dsv16x_gy_data_rate_set(&sensor.dev_ctx, LSM6DSV16X_ODR_AT_960Hz);
	if (ret) {
		LOG_ERR("lsm6dsv16x_gy_data_rate_set (%i)", ret);
	}

	/* Mask accelerometer and gyroscope data until the settling of the sensors filter is completed */
 	filt_settling_mask.drdy = PROPERTY_ENABLE;
 	filt_settling_mask.irq_xl = PROPERTY_ENABLE;
 	filt_settling_mask.irq_g = PROPERTY_ENABLE;
 	ret = lsm6dsv16x_filt_settling_mask_set(&sensor.dev_ctx, filt_settling_mask);
	if (ret) {
		LOG_ERR("lsm6dsv16x_filt_settling_mask_set (%i)", ret);
	}
	lsm6dsv16x_filt_xl_lp2_set(&sensor.dev_ctx, PROPERTY_ENABLE);
	lsm6dsv16x_filt_xl_lp2_bandwidth_set(&sensor.dev_ctx, LSM6DSV16X_XL_STRONG);

	qvar_mode.ah_qvar_en = 1;
	ret = lsm6dsv16x_ah_qvar_mode_set(&sensor.dev_ctx, qvar_mode);
	if (ret) {
		LOG_ERR("lsm6dsv16x_ah_qvar_mode_set (%i)", ret);
	}

	pin2_int.drdy_ah_qvar = PROPERTY_ENABLE;
	ret = lsm6dsv16x_pin_int2_route_set(&sensor.dev_ctx, &pin2_int);
	if (ret) {
		LOG_ERR("lsm6dsv16x_pin_int2_route_set (%i)", ret);
	}
	return 0;
}

 

 

As a side question, I saw that the LSM6DSV16BX sensor is capable of outputting the QVar data in FIFO. What are the differences between the two versions LSM6DSV16X/LSM6DSV16BX ? I will look into that component's datasheet to see if I can find some, but it would be a nice help :)

Thanks in advance for your help

Nicolas Goualard

Best answer by NicolasGoualard

The structures related to int1, int2, sflp and settling mask were not initialized, so random values could be present. When I initialized these structures to 0, it worked fine.

1 reply

NicolasGoualardAuthorBest answer
Associate II
September 28, 2024

The structures related to int1, int2, sflp and settling mask were not initialized, so random values could be present. When I initialized these structures to 0, it worked fine.