Skip to main content
Visitor II
August 24, 2024
Question

lsm9ds1-gyroscope

  • August 24, 2024
  • 1 reply
  • 810 views

Hi,

I have an application with LSM9DS1 sensor and I expected that when I change LSM9DS1 sensor position from horizontal to vertical value will change but changed only when sensor was moving but after that valus comes almost same for horizontal or vertical position.  I don't understand how its working. I have smole expirience with sensor ADXL345 and this sensor on horizontal possition give me values arround 0, on vertical position values is arround 256 (- +) and that is clear for me.
Thanks for any explenation - helps.
Regards Jarek

    1 reply

    Federica Bossi
    Technical Moderator
    August 29, 2024

    Hi @JarekG ,

     

    You can follow our official example on Github to implement the code to read the LSM9DS1 output.

    Are you reading the accelerometer outputs?

    In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.